Other Parts Discussed in Thread: UCC28780,
I found two planar transformers that I want to use in an ac-dc converter.
750341145 and MTPL-2516.
Universal input: 90-265 Vrms AC
Output: 12VDC, 1A
Primary winding of transformers will see bridge rectified pulse DC.
UCC28742 can drive MOSFET switching at maximum 105Khz. Similar case with UCC28740DR which is what WEbench tool suggests when I try to simulate a necessary circuit. Webench doesn't account for a planar transformer, which may require higher than 200Khz of frequency.
Does it mean I have to use an SMPS controller such as UCC28780? The latter requires complex circuits, whilst I want small & simple schematics, such as the one that's offered by UCC28742.