This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25155: VOL problem between BQ25155 and CC2642R

Part Number: BQ25155
Other Parts Discussed in Thread: CC2642R

We are using the MCU mentioned above (CC2642R) and charger (BQ25155). the problem is with the VOL value of BQ25155. 0.525V is the highest GPIO output voltage reliably interpreted as low by BQ25155. However, VIL(Highest GPIO input voltage reliably interpreted as a Low) is 0.42V. So 0.525V won't be interpreted as low by CC2642R.

How to solve this problem?

Is it even an issue? If it's not an issue?