This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25616: Can BQ25616 support ship mode?

Part Number: BQ25616

Hi team,

my customer need a 1cell charger, the spec as below:

input 5V~6V

battery voltage is 3.7V, system voltage is 5V; charger current is 1A; need power path management and ship mode

I recommend the BQ25616, but I'm not sure if it is the best solution. could you give some recommendations with I2C interface and standalone interfance?

thank you.