This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM26480: LM26480

Part Number: LM26480


Hi,

The Case we used is as follows:

SW1: 0.9V/135mA

SW2: 1.8V/150mA

1.How long is Start-Up to ready in these two cases?

2.Does Turnon time indicate the position of the arrow as shown below?

Thank you

  • Please share a schematic of your design so I can answer your question.

    Also, which orderable part # of LM26480 are you using?

  • Turn-on time is the same as ramp time.

    It is the time from VOUT = 5% to VOUT = 95% after the EN pin is set high.

    There is one exception: 

    "The enable signal may be employed immediately after VIN is applied to the device. However, VIN must be stable for approximately 8 ms before enable single be asserted high to ensure internal bias, reference, and the flexible POR timing are stabilized. This initial delay is necessary only upon first time device power on."

    If EN is tied to VIN, then there will be a delay of approximately 8ms from when EN is high to when the SW1/2 converter turns on. However, the TON spec is still valid from 5% to 95% VOUT.