This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Temp accuracy spec range for internal temperature sensor

Part Number: BQ27426

As title, I think Fig4 in DS is used to explain the accuracy for internal temperature sensor.

My questions are 

1. Based on this figure, the best accuracy is at ~10degC. But normally, it should be at 25degC normal temp. Thus I would like to double confirm if this figure is true.

2. If we perform a temp calibration at 25degC, does it means the curve will be corrected. In the other hand, 0% is at 25degC and the curve is shift to higher and until 25degC is 0% error.  

  • Hello,

    The Datasheet should be correct: the lowest error is at -10degC. I will double check though.

    The error at each temperature reading would be based on your calibration temperature, this could compound the error from the current temperature and your calibration temperature error.

    Sincerely,

    Wyatt Keller

  • Hello,

    1. Please help to confirm this figure#4 is correct. 

    2. Seems like I didn't get answer for question#2.

    Assume temp error @ 25degC is 5% and temp error @ 0degC is -1%. After perform a calibrate process at 0 degC, supposedly the temp error will be 0%.

    Does it mean temp error@25degC will be 5+ 1 = 6%?

  • Hello Beginner,

    1. Figure 4 was measured on a bq27426 EVM. Do you have any specific measurement issues you are seeing on the bq27426?

    2. No, we would really need to measure the temperature on a per board or per IC basis.