Part Number: LM62440-Q1
Hello,
I'm looking for some clarification on the efficiency graphs for this part. The 3.3V ones make sense to me as the graphs match up at the end of the auto-mode current scale since the device is essentially operating in PWM. The 5V graphs don’t do this, and I am not sure which plots are correct. Specifically 24Vin to 5Vout at 3A, in AUTO mode the graph shows ~91% and in FPWM it shows around 83%. Is there a reason the 3.3Vo graphs converge and the 5Vo ones don't?
Thanks,
Michael