This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138: Seeking a 1kw digital power reference design case based on UCD3138

Part Number: UCD3138


Hello,

I want to use UCD3138 as a 1kw digital power supply with an input voltage of 300V and an output voltage of 48V.

Hope that the volume is as small as possible (such as half brick), as few components as possible (less than 200), and the efficiency is as high as possible (such as 96%).

I see UCD3138 has many reference cases, such as full bridge, phase shifted full bridge, LLC, etc.

Don't know which reference case is most suitable?

Thank you.