This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: BQ24610 supports 20A input adapter current

Part Number: BQ24610


Hi,

Just confirm with you if BQ24610 can support 20A input adapter current by changing Rac to 5 mΩ?

Best Regards

Sean Zhang

  • Hi Sean,

       Theoretically BQ24610 is a charge controller, so it can support higher charge currents. However the internal gate drive strength is limited. If using high current applications, higher Id rated FETs are required, which usually have higher Qg. This would cause increased gate driver loss. Also as conduction loss is much higher, extremely careful layout is required for thermal dissipation. It is not recommended to use BQ24610 above the 10A max charge current rating.

    Yes, changing RAC to 5mohm would increase the input current limit (assuming 2V sourced on ACSET pin) to 20A.