I have an application using the bq20z75 in a non-removeable application. I need the pack to go to sleep. What setting should I use or does it go to sleep at all when non-removeable? There is no SMBus communication except when it is in the charger. The pack is designed to stay in the unit (a robot) for long periods of time and if the pack is not in use, it needs to shut off. In the unit I have the bus lines pulled down with 1M resistors.