Other Parts Discussed in Thread: TPS5420, TPS2541
I noticed that the GND pin for the TPS5420 EVM board is not connected directly to the C4+C1 input cap ground plane but first connects to the catch-diode (D1) plane and then out to the main C4+C1 plane.
However, the board layout recommendations in the TPS5420's datasheet (Figure 9, Design Layout) show the GND pin being connected directly to the C4+C1 plane and the D1 plane.
Which method would you recommend for a new board layout? I'm guessing that the EVM's method is preferred as the EVM is shipping now and the datasheet is from 2007. But, it also seems that not also connecting GND directly out to C4+C1 keeps D1's noisy, high current path localized and away from the rest of the circuit. I wanted to be sure though.
Thanks!