Dear TI engineers,
I am considering using the LMZM33606 power converter to provide 12V from a 24V source.
This converter is supposed to provide up to 6A, which would equal 72W at 12V but on datasheet's main page, is written "Up to 50-W Output Power at 85°C, No Airflow"
1) Is it a continuous output power based on efficiency, temperature and power dissipation?
2) Is the converter able to provide up to 72W for a few seconds once in a while, if the mean power is < 30W?
3) Is the converter able to provide more than 50W continuously provided the cooling is sufficient?
Thanks in advance for your help!
Regards