Hi
I am using a LM5060 to drive 2 200W brushless DC motor in a automotive robot, but there is high oscillation appear at the output.
Usually the oscillation happens when the robot stop from moving. I wonder what may cause such thing happen?
This oscillation affect the RS485 line of the motor and cause it hang up.
Since the motor has 6000uF capacitance in total, I use the driver to control the inrush current.
The P-MOSFET is to block the reverse current flow if the robot is moved by force manually when the robot power off.
C13 is not installed component.
I tried to removed the P-MOSFET part, but the oscillation still happen.
Yellow is the current of one motor
Green is the voltage of the motor
Blue connected to nothing, oscilloscope is internal grounded. (and the ratio was wrong, please x10 the amplitude)
Usually the oscillation happens when the robot stop from moving, but sometime it happen while moving.
Also, if I lift up the robot and left the motor run in no load, it seems that oscillation does not happen.
If anyone could help, I would be really appreciate.
Thanks