This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I would like to increase the output current of the LED string.
Is it possible to do this with below connection ? Do you have any issues with it ?
Regards,
Ryan
Hi Ryan,
Yes, that ok. and for each channel of TPS61196, it can continuously output 200mA, so I would suggets to combine 3 channels together to driver 500mA.
BR
Sean
Hi Ryan,
No, thst for pulse current with 400mA, we only recommend for maximum 200mA for each channel so for 500mA, we recommend minimum 3 channels.
BR
Sean
Hi Sean,
I plan to drive 5 LED strings with each string containing 28 LEDs.
The current for each string are as below:
Given this requirements, please help confirm that using part TPS61196 is not suitable in our design.
If yes, can you help advice another part that meets this requirement ?
Regards,
Ryan
Hi Ryan,
I'm sorry that TPS61196 can't set the different full-scall current for each channel, and it is better not to set over 200mA for each channel, I would suggest with the solution with several TPS61196.
BR
Sean