This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: Questions about pins and functionality

Part Number: BQ25601


Hi all,

it's the first time I use this chip and I don't understand some functionality of some pins.

I follow the connection scheme of the datasheet at figure 40 but something is not working.

The only difference is that i don't need to use the USB: I have an external power supply at 12V and, at the input of my device, I use a DC/DC converter to obtain the 5V level.

Then I just want to use that 5V level as the Vbus at the input of the BQ25601 and:

  • when the 12V power supply is ON, the BQ25601 must charge the battery (at the same time i need to use the 5V to supply the whole device);
  • when the 12V power supply is OFF, the BQ25601 must give the 5V at the output of the chip in order to supply the whole device.

Actually, when I turn on the 12V power supply, my DC DC Converter at the input stage gives the 5V level and I measured this signal at the VBUS/VAC pins of the BQ25601.

It seems that th BQ25601 didn't work: no output at the SYS pin and the battery is not charging, even I put the /CE pin to the GND.

I tryied to put also the PSEL to the GND but the output of the BQ25601 is still to 0V.

Maybe I'm doing something wrong?

Please, could you help me to understand?

Thank you in advance

best regards,

Michele