This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25942A: Absolute Maximum Ratings of Vout without VIN

Part Number: TPS25942A

Hi team,

 

Could you kindly advise the abs max of Vout without Vin ?

In my understanding, even if Vin is not applied, abs max of Vout is the same in the datasheet.

 

Please let me double check.

Thank you and best regards,

Michiaki

  • Hi Michiaki,

    You are right ! The Abs Max rating of Vout for TPS25942A with  or without Vin is the same as mentioned in the datasheet.

    If Vout is a function of Vin, the datasheet spec would have been something like 'Vin + 0.3V'.

  • Hi Michiaki,

    You are right ! The Abs Max rating of Vout for TPS25942A with  or without Vin is the same as mentioned in the datasheet.

    If Vout is a function of Vin, the datasheet spec would have been something like 'Vin + 0.3V'.