Other Parts Discussed in Thread: LM73606
Hi team,
Would you please advise if there is any concerns in sequence if enable is earlier than Vin?
Or this part doesn't have power up/down sequence limitation?
Thank you.
Regards,
Allen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Would you please advise if there is any concerns in sequence if enable is earlier than Vin?
Or this part doesn't have power up/down sequence limitation?
Thank you.
Regards,
Allen
Allen,
We do not recommend applying a voltage to EN before VIN. Devices typically have ESD diodes from each pin to GND and to VIN so applying a voltage to EN before VIN may cause current to flow through that ESD diode (which is not rated for continuous current).
-Sam
Eddie,
You need to check if the LM73606 input voltage rises faster than the low-passed EN signal so that it does not violate the absolute maximum spec of the EN pin which is VIN + 0.3V. Limiting the current into the EN pin would be a more reasonable solution but still not recommended. ESD diodes are not meant for continuous current.
-Sam and Jerry