I am currently working with the TPS1HA08 chip and I believe i am having a fault error situation. Once the chip is enabled, it outputs the correct voltage and reads the appropriate current (both the power supply and SNS pin). However, the VOUT pin quickly (~300ms - 500ms) disables and will not turn back on until the Enable pin has been reset. All resistance and capacitance values are that of suggested via the data sheet relevant to this chip.