This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1101A-SP: Unconnected pin 12 (GND pin) of TPS7H1101A-SP die version

Part Number: TPS7H1101A-SP

Hi Team,

Our customer would like to confirm if the pin 12 of TPS7H1101A-SP die version must be connected to GND?

The customer is having some loading issues on the part. Basically, when they run GTX on the output line, the 1.0V drops. They suspect this disconnected pad is the culprit. Must it be connected to GND? Or will it function properly left unconnected?

Thanks,

Jonathan