This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95: BQ20Z95 - Could MaxError be "Reset"?

Part Number: BQ20Z95

Dear Sir,

I have a question, is MaxError able to be "Reset" to 1%?

I have a battery pack and its MaxError is 5%, the cyclecount is 98 times.

Thank you very much

Renee

  • Hello Renee,

    The MaxError will be reduced to 1% when both Qmax and Ra are updated. After each cycle the gauge has been increasing the MaxError by 0.05%. The error must increase because over time the Qmax changes and it needs to update to stay accurate.

    Sincerely,

    Wyatt Keller