we met one cell imbalance issue when charge terminate.
Cell 0 voltage: 3.34
Cell 1 voltage: 3.37 V
Cell 2 voltage: 3.84 V
State of charge: 94.00 %
SOC can't reach 100% in this case.
After check our config, our taper current is 800mA, but default value is 150mA. How to define this taper current? smaller taper current or bigger taper current could be better for cell balance?