Hello
i am using BQ25713EVM-017 Module to charge 10 S 1300mAh 12V Battery
and i changed Disable Low Power Mode for ADC
MAX CHARGE VOLTAGE : 12592 mA
MIN SYSTEM VOLTAGE : 9984mA
it is my module config
the problem is that ADC IDCHG is always 0 mA even thought only Battery without DC
and i have question one more ..
when ADC VBAT / ASYS is above Max Charge Voltage , Does ADC ICHG Value become 0 mA ??
i mean , i connected DC to charge battery , and Charge Current Register also was 320mA , Watchdog Timer was disable
and when i check ADC ICHG Value , it was 0 mA
how can i know that battery is full ??
thank you