This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381A-Q1: could we reduce feedback res to reduce quiescent current?

Part Number: TPS65381A-Q1

Hi Team,

May I ask why these two res choose 43.2 and 80.6 so small value? Could customer change to bigger, such as 40k80k or 4k8k ohm?

Because customer need to keep quiescent current less than 700uA when in sleep mode and VDD is 2V.

If the res is 40 and 80 ohm, the Iq will be very large...