This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
I need a negative output voltage(-0.8V_out) for RF ADC application which only consume 200mA load current.
The ripple performance have to within +/- 24mV.
Is TPS62561 a right solution? (It's acceptable, if we need to design an extra inductor/bead to improve ripple performance)
Application:
3.3Vin to -0.8Vout @ 200mA load current.
Regards,
Ben
Hi Ben,
A buck converter in an inverting buck-boost topology can be made by following this reference design: TIDA-01405, different buck converters can be used in place of the one given in the reference design.
The least time consuming design should be to use a module with an integrated inductor such as the TPS82084.
For a converter without the integrated inductor (a less expensive option), I could recommend the TPS62821. Or for an even more cost-optimized approach the TLV62568A could be a good solution as well.
Note that the TPS62561 you mentioned has a minimum Vout of 0.85, so in the inverting configuration it cannot reach the -0.8V of your specifications.
Kind regards,
Davor
Hi Ben,
Since we continued our communication over e-mail, I will close this thread.
Regards,
Davor