Hello community,
I am currently using a TLC59108F as PWM controller to drive LEDs, DC motor, ... That's working as expected, except the PWM frequency is greater than told in the datasheet : I can observe a frequency of 107.9kHz (mean period is 9.268µs) with my oscilloscope.
I need to mention that I wait at least a few seconds after setting OSC bit in MODE1 register to update PWMx and LEDOUTx registers.
The datasheet doesn't mention min/max PWM frequency, do you have any idea what would be the tolerance ?
Thanks,
Kevin