This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR50410: Webench

Part Number: LMR50410

We're interested in new device of the LMR50410 for below conditions. But It looks it doesn't work on the WEBENCH. What's the problem with? 

If LMR50410 is not a right part, please advice other device. thanks. 

Condition: 

Input Voltage: 14V - 16V (26V is max. rating)

Output Voltage: 12V

Output Current: 500mA

Regards

Brian W