This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM53601-Q1: LM53601A: feed forward cap on the FB pin

Part Number: LM53601-Q1

Dear sir,

We want to improve the peformance of our LM53601AQDSXRQ1 circuit

Is it possible to add a feed forward capacitor between the FB and the Vout pin?

And what is the recommend value of it( a little soft start(<300us) phenomenon is acceptable)

our current setting are as followed

Vout=3.3V

feedback divider resistor value are 100k and 43.2k 

input cap:>30uf

inductor: 4.7uF

output cap:>20uf

Thank you very much for the help

Best regards

Joe Huang