This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161: Low side current limit operation and max sinking current limit value

Part Number: LM5161


Hi team,

 

In the datasheet of 7.3.7 Current Limit, current limit operation is described but is it apply to low-side current limit as well ?

Or is it only for high-side current limit ?

If 7.3.7 is for only high-side current limit operation, could you kindly advise the low side current limit operation ?

 

 

Sinking current limit is defined typ 3A in the datasheet.

Customer see sinking current of max 4.7A in their application.

 

Could share the number of max sinking current limit ?

 

Thank you and best regards,

Michiaki