This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS43060: Rsense value

Part Number: TPS43060


Tool/software: WEBENCH® Design Tools

Hi Team,

I use WEBENCH to do the simulation, but Rsense confused me.

My condition is input 5V -> outpu 7V/0.15A in 30C and the Rsense showing in WEBENCH is 330m//330m=165mohm but I use datasheet formula(10) to get Rsense is 375mohm. 

I think these two value is so different. how could I choose?WBDesign62 (1).pdf