This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61023: Current Limit is not happening

Part Number: TPS61023

Hello,

I have designed a board using TPS61023 IC. This is used for Mobile Charger application. Input and output specifications are mentioned below:

Input Voltage - 2.8V - 4.2V

Output Voltage - 5V

Output Current - 1A

The Inductor I have selected is 2uH. 

When I am increasing the load current above 1A, current limit operation was not happening. It is happening at 2A. When the load current reaches 2A, output voltage decreases.

But I want this to happen when the load current reaches 1A.

Could you please help me to resolve this issue.

Regards,

Jilna

  • Hi Jilna,

    Thanks for reaching out.

    The boost converter TPS61023 employs a valley current control method and limits inductor valley current at 3.7A typically. And minimum sepc is 2.7A. 

    Because inductor current equals input current for a boost converter, so this device is limiting the input current at a certain value, not the output current. With different input voltage, the maximum output current capability is different.

    You have to add a load switch after TPS61023 output.

  • Hi Sir,

    Is there any alternate way to solve this issue, other than adding a load switch?

    Can I adjust the Inductor value?

    Regards,

    Jilna Jayan

  • Hi Jilna,

    It's not possible to control the output current. Boost converter is only limiting the input current and it's current limit accuracy has bigger variation compared to accurate load switch device. Sorry.