This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: bq25895 VSYS drop to 0

Part Number: BQ25895


Dear team,

During customer's test, there was one board that VSYS will drop to 0 @55 degree C. Others are normal. VBUS is not on when fault happens. If add VBUS, the VSYS will become normal. It seems BATFET is off, I could make sure that battery voltage is about 4.0V and no over-current happen. 25 degree C has not seen same issue.

Thanks.

Best regards,

Sammi