Part Number: TPS61022
Hello,
I have a customer asking the following question:
"I tested the TPS61022 and I am getting a power drop when I have a 1.5A current spike with Vin<2.65V and Vout=5.1V.
Do you have a different boost with higher current drive capabilities?
It needs to work:
Vin 2V
Vout 5-5.2
Iout 1.5-2A for 10mSec with drop no more than 0.5V"
Do we have such a device to offer?