Other Parts Discussed in Thread: LMR36006
I am considering using the LM5166 in a design where it will sometimes act like an on/off switch for LEDs. The LED forward voltage is about 9V, so my idea is to set the LM5166 Vout to 12V and allow it to enter 100% duty cycle mode. The current is limited upsteam, but it can be a little higher than 500mA - maybe 600-700mA. I am unclear what the LM5166 maximum output current can be in this mode. Is it 500mA, the typical max output current of the part? Or, since the part will not be switching, is it 1250mA, the high-side switch limit? Or somewhere in between?