Part Number: LM3644
Hi Team,
Just a few question about LM3644 LED driver,
1. Can we drive 1.5A from each LED channel (1.5A + 1.5A, total of 3A) ?
2. If we are not using TX, STROBE & Torch pins, can we left it floating?
Thanks you,
K. Rajesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM3644
Hi Team,
Just a few question about LM3644 LED driver,
1. Can we drive 1.5A from each LED channel (1.5A + 1.5A, total of 3A) ?
2. If we are not using TX, STROBE & Torch pins, can we left it floating?
Thanks you,
K. Rajesh
Hi Sean,
Thanks for the details !!
One more doubt, how to determine power dissipation of LM3644 IC?
We are using 5V as input, driving 1.2A current from each LED channel (so totally 2.4A ) and LED forward voltage is 3.25V.
For thermal analysis, we need this power dissipation value.
Thank you
k. Rajesh
Hi Kora,
I'm sorry that It is difficult to calculate the power loss, the most accurate way is to test with the detail application spec, you can request the LM3644EVM from TI.com.
BR
Sean