When UCC28610 detect brown out threshold, how fast controller will stop switching? Since it did not specify on datasheet, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When UCC28610 detect brown out threshold, how fast controller will stop switching? Since it did not specify on datasheet, thanks.
Hello John,
The converter will not shut down to a fault unless it has occurred in 3 switching cycles. So the input under voltage needs to be detected in three consecutive switching cycles.
Even though the delay is not specified the ZCD delay of 150 ns is specified. So the delay time after initial brownout could vary from
3/fmin + 150ns to 3/fmax + 150 ns.
Also note when the line is removed there will be a delay due to the bulk capacitor discharge.
dt = (Cbulk/Iin)*(Vin - Vin@BrownOut.
So the total variation would be
(dt+3/fmin + 150ns) to (dt + 3/fmax + 150 ns.)
Regards,
For overload detection, is it the same converter will not shutdown to a fault unless it has occurred in 3 switching cycles?