This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for buck single lithium ion battery charger with smallest form factor

Other Parts Discussed in Thread: BQ25618

Hello Ti Team

I am looking for latest single cell buck converter Battery charger with  smallest packages.

1. System Current: 1A

2. Battery Charging current : 0.5A

3. Input : 5.5V max

4. Chemistry : Li-ion/pol

5. NTC support

6. Host control : I2C

7. Configurable output battery voltage

Thanks

Shekhar

  • Hi Shekhar,

    Thanks for the inquiry. Please feel free to look at BQ25618, this addresses all you requirements, also provides 95.5% efficiency when charging at 0.5A and the battery voltage is configurable from 3.5V - 4.52V. 

    Please feel free to ask any further questions.