This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570EVM-206 :BQ25570EVM-206 : VOUT Q&A

Part Number: BQ25570EVM-206
Other Parts Discussed in Thread: BQ25570

In the datasheet of BQ25570, I identified VOUT= VBIAS* ((ROUT2+ROUT1)/ROUT1).

I think ROUT1 and ROUT2 are R9 and R10 on the BQ25570-EVM board.

So I would like to know if it is possible to replace R9 and R10 on the board with a different value to adjust the VOUT to any value I want. (Of course, within the range of possible VOUT in the data sheet specification.)

If VOUT value can be adjusted, the data sheet indicates that the sum of R9 and R10 should be less than 13M ohms, but can it operate normally even if the sum of R9 and R10 is about 8M ohms or 7M ohms?