UCC28610 datasheet block diagram shown there is comparator close to MOT pin with 3V reference voltage.
What is the function for this comparator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC28610 datasheet block diagram shown there is comparator close to MOT pin with 3V reference voltage.
What is the function for this comparator?
Hello John,
It appears that the block diagram is not very clear on this function, and I believe that the comparator function on MOT is not strictly drawn as to its function.
However, I interpret it to mean that that comparator detects whether the MOT voltage is either above 3V or below 3V and adjusts the Fault response as Latch-Off or Retry respectively, per Figure 19 of the datasheet (page 15). There must be a current coming out of the MOT pin that sets up a voltage (Vmot) across the MOT resistor to GND. For Rmot below 120kR, the Vmot < 3V and for Rmot > 120kR, the Vmot > 3V.
Simple math suggests that the current is 3V/120kR = 25uA. I believe that Vmot also generates a separate timing current (not shown) that sets the maximum on-time. The comparator also changes the gain of an internal current mirror by a factor of 5 to generate the same timing current from the higher resistance range as it does with the lower resistance range. You can see that a 30k-to-100k range has the same timing range as the 150K-to-500K range. This way a single pin performs 2 programming functions: determining maximum on-time and selecting retry vs. latch-off fault response.
The block diagram is overly simplified, I believe.
Regards,
Ulrich