Other Parts Discussed in Thread: LM74800-Q1
Tool/software: WEBENCH® Design Tools
Dear Sir,
I want to use LM74800-Q1 for Hotswap between Source @ 1 and Source @ 2
Source @ 1: SMPS Power Supply: 48 V DC
Source @ 2: Battery Volatage: 48 V DC
Load Requirement : 48 V @ 60 A
I don't want any delay in change over from Source @ 1 to Source @ 2.
My load should not see any disturbance in change over.
My first priority is Source @ 1. if source @ 1 fails, Source @ 2 should take over the load requirement.
I request you to check LM74800-Q1 is fulfilling my requirement.
Can you share the eagle library file? So that I can develop a Schematic.
Please confirm when it is available for purchase
Regards
Murthy