Other Parts Discussed in Thread: TIDM-1007, TIDA-010062, TIDM-02008
Hello,
We have two power-electronics questions about TIDA-00961 & TIDM-1007. These are;
- TI Designs: TIDA-00961 (High-Efficiency, 1.6-kW High-Density GaN-Based 1-MHz CrM Totem-Pole PFC Converter Reference Design) is primarily used to rectify AC mains to 400VDC. The question is; can we use that design to rectify the AC mains to 48VDC? Will we still be able to achieve proper PFC?
- If the target is to us achieve rectification of the single AC main with adjustable DC output. Do you recommend using TIDA-00961 or TI Designs: TIDM-1007 (Interleaved CCM Totem Pole Bridgeless PFC Reference Design Using C2000™ MCU)?
Regards
Sam