Other Parts Discussed in Thread: TPS92691
Hi Team, Could not the function just be done with resistor divider in this diagram ( fig 26 Q4) ? Also just wondered if there was an undervoltage circuit for this part?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team, Could not the function just be done with resistor divider in this diagram ( fig 26 Q4) ? Also just wondered if there was an undervoltage circuit for this part?
Hi
You need Q4 to level shift and convert the differential voltage between LED+ and LED- to single ended voltage referenced to ground. The resistor divider would only give you the LED+ voltage
-Sumeet.
Many thanks, I guess what I was also trying to understand why is it important to measure the overvoltage across the led terminals, is not the failure condition that you should be most worried about an open string and Vled+ going too high? If there was a led that shorted short then the voltage between the led terminals would decrease?
Hi Ajayt,
The feedback to the OV pin is only use to protect an over-voltage condition and not a one LED short out of a string of LED's. The transistor level shift gives the actual differential LED+ and LED- voltage and if there is one LED short out of a string then the voltage would decrease but the TPS92691 will not be able to detect this one LED short failure from a string of LED's.
Thanks Tuan