Hi all,
In my application I have the need for One-out-all-out across across multiple TAIL function boards. My question is whether or not there is a recommendation on connecting fault together between multiple boards to achieve one-out-all-out. Is it recommended or not?
The right hand tail, left hand tail, and body side tail all need fault connected together. Right hand tail and left hand tail are close to each other but body side tail could have ~1m cable harness.
If we cannot connect FAULT together over these lengths then is there a recommendation on how to help achieve OOAO in this situation?