Part Number: LM5001
Other Parts Discussed in Thread: LM5180, LM5180-Q1,
Tool/software: WEBENCH® Design Tools
Hi All,
I am using Lm5001-q1 IC for design of 2W power supply. I have 4 output windings in which 3 are isolated and 1 is non isolated. I am taking the feedback from the non isolated winding to make it as a non isolated flyback converter.
The input voltage is 12 volts and I am expecting 7 volts across all the secondary windings.
But when the input is connected, I am able to get only 3.4volts at the output winding.
Checked with the transformer and it is fine.
The duty cycle is 20 percent and has saturated.
Can anyone please suggest what moght have gone wrong?