Other Parts Discussed in Thread: TPS563249
Is there any voltage regulator with I2C bus so that its output voltage can be programmed as any value (e.g. 3V~6V @ 2A)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS563249
Is there any voltage regulator with I2C bus so that its output voltage can be programmed as any value (e.g. 3V~6V @ 2A)
Jack,
We have some devices, but they program to lower output voltages like 0.8 to 1.95V. Are those of any interest? Otherwise, you can use a digital potentiometer as the lower resistor divider to set the output of many converters. Most of our full feature devices are designed around much higher output currents. Let me know if any of those are of interest to you.
Thanks John,
Unfortunatelly 0.8~1.95V voltage range is too low for me. So I will use DAC chip to output voltage to some regulator IC (e.g. TPS563249) VFB pin so as to adjust the output voltage.
Thanks again
Jack