This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to remove ripple in supply using regulators

Other Parts Discussed in Thread: TPS793, TPS7A49

Hello,

I have a power supply which gives 12V DC, 120mA with ripples of about 200mV (at a frequency of 60 Hz). I want a 3.3V clean supply using this source.

I tried using the high PSRR solution from TI: TPS79333. But, it didn't remove the ripples, and consumed more than 120mA. I have also tried other LDO regulators, Zener diode, different capacitances after a 3.3V LDO. But, the ripple remains.

Can someone please help me figure out how to remove this ripple?

Thanks,
SF 

  • Hello SF,

     

            TPS793 will not be able to even take 12V at Vin (its maximum rating for Vin is 6V). I highly recommend using TPS7A4901DGN for this application (Vinmax=36V).

           Also, bear in mind that, for this application, you are looking at ~1W of power dissipation  [ (12V-3.3V)*0.12A = 1.044W ]. You need to take this into consideration when selecting the right package for your LDO. Again TPS7A49 comes in a MSOP-8 package with PowerPad that is able to dissipate ~1.8W at room temperature.

     

                      Victor.

  • By the way, when there is a 60Hz signal in  your system, consider checking your grounding and/or shielding your application. Sometime ground loops or high impedance nodes (long cables acting as antennas) may cause this kind of problems.

     

    Hope this helps,

     

               Victor.