Hello,
I would like to remove the I2C pull-up resistors on the EV2400 as my board has them incorporated.
On my board I pull the I2C lines up to a single cell Li-Ion battery (3.0 - 4.2 V).
Is this as simple as removing R13/R14 from the EV2400? It's not evident what the value of VPUV.2 is as it is controlled by a digital potentiometer and I do not want to exceed the pin ratings of the EV2400's I2C level shifter (U5).
Thanks,
Kevin