Hi,
I need experts help.
I use a Li-ion battery with 5Ah for a 18V power tool and want to load it with a solar panel. Therefore I'm looking for a microcontroller (best would be circuit layout) which is suitable for this application. I intended to use a solar panel with the following features:
- max. power: 50Wp
- Voc: 22,3V
- Vmpp: 18,5V
- Impp: 2,72A
- Isc: 2,84A
Can you suggest me a microcontroller for the battery management, resp. load regulator for this application?
Best regards
Matthias