I want to use TPS62840YBG with a lisocl2 battery as input to power a lora module sx1276 module with current peaks of 250mA, which Ferrite beads do you recommend?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use TPS62840YBG with a lisocl2 battery as input to power a lora module sx1276 module with current peaks of 250mA, which Ferrite beads do you recommend?
Hi Domenico,
Unfortunately, we will not be able to recommend any ferrite bead as this is not directly part of the recommended BOM for TPS62840. If you need to use a ferrite bead for your application, you will have to choose one based on your filter requirements and test it by yourself. We do not have any test circuits using ferrite beads to share with you at the moment.
Please let me know if I can help you otherwise.
Regards,
Febin