Part Number: BQ27750
Hello. In my circuit, I added a 0.1 uF capacitor in parallel with the NTC-thermistor (B57861S0103F040), wrote the coefficients in the temperature model (they work fine on bq4050). The internal temperature is measured correctly and shows -40, but the cell temperature is 10 degrees higher, that is -30 C. I think that this is the case in the capacitor, which I installed additionally. Please tell me, is it possible to put a capacitor in the measuring circuit of the NTC-thermistor? And is it possible to somehow compensate for the presence of a capacitor so as not to evaporate the capacitor?