Part Number: BQ40Z50-R3-DEVICE-FW
Hi TI Team,
I have couple questions about Reserve Cap-mAh. When I set e.g. 500mAh to reserve, I found that the full charge capacity will decrease pretty much the same amount right away. In this case,
Do I need to decrease the Design Capacity setting with the same amount (500mAh) as well?
When I change the setting for either Reserve Cap-mAh or design capacity, do I need to re-run a learn cycle to generate a new golden sample?
I also found that if not change the design capacity, ASOC is deceased but SOH is still 100%. Why SOH is not affected since SOH ~= FCC/DC while FCC is decreased?
I would appreciate it very much if someone could answer my questions!
Best Regards,
Zhihan