Normal 0 21 false false false MicrosoftInternetExplorer4
Hello,
I’m using a bq27510 v.1.11. The chemistry profile chosen by bqEasy (0.971) is the ID237.
Is this chemistry profile a part of the golden file? When I update the bq27510 v.1.11 for production with the golden file do the devices know this chemistry? I have the impression that this chemistry was not part of the list in earlier versions.
I did not plan to update the firmware version of the devices because this adds some complexity for production but only the golden file.
Any answers are welcome.
Thanks in advance,
Matthias